Technical FAQs

Ask a Question

What are the repair parts for a QMB363HW, Series E1 (E01)?

Issue:
Repair parts

Product Line:
QMB Branch Switch

Environment:
Repair parts

Cause:
Maintanance

Resolution:
Only the parts listed below are considered field replaceable:
Complete Arc Suppression Assembly - 3 part numbers required:
(1) Arc suppressor Assembly (1 required) - 4052021450
(1) Arc Shield (top cover) (1 required) - 4052017302
(2) Push nuts (2 required) - 2330241601
Load Base Assembly (1 required, includes lugs) - 4052021650
Load Base Mounting Screw (2 required per load base) - 4020506501
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101851
Lug Mounting Nut (per lug) - 2342702001


 
Was this helpful?
What can we do to improve the information ?