Technical FAQs

Ask a Question

Can an EZML312400 (3phase in - 1phase out branch device), connect with an EZM11600TB 1 phase main device.

The EZML312400 branch device is a 3 phase in ONLY device and WILL NOT connect to the EZM11600TB. See Digest 172 pages 2-8 thru 2-13.


CTA-ID : 2365
Was this helpful?
What can we do to improve the information ?