Technical FAQs

Ask a Question

What are the repair parts for a PAK61CTG, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161
Interior Trim - 4054025001
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4054020151 (Includes Base Assembly, Circuit Breaker(s) and Receptacles(s) below.
Base Assembly - 4054011450
Circuit Breaker - QO120GFI and (2) QO130
Receptacle - 4054001450 (125 volt/20 amp) and (2) 4054004450 (125 volt/30 amp)
Receptacle Mounting Screw - 2190312160 (1 req`d for the 125 volt/20 amp receptacle)
Receptacle Mounting Screw - 2159412120 (3 req`d for each 125 volt/30 amp receptacle)
Ground Bar - 4023017155
Ground Bar Mounting Screw - 4020594401
Neutral Bonding Screw - Not Applicable
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 5404
Was this helpful?
What can we do to improve the information ?