Technical FAQs

Ask a Question

Can you identify safety relay 8932 GSK3LB?

Yes E-stop relay. Drop 8932 Class and the GSK3LB`s are on the system. Will have to add input voltage for complete part number.


CTA-ID : 5300
Was this helpful?
What can we do to improve the information ?