Technical FAQs

Ask a Question

What are the repair parts for a QMB226WT3, Series E1 (E01)?<br />

Only the parts listed below are considered field replaceable:
Complete Arc Suppression Assembly - 2 part numbers required:
Arc Suppressor Assembly (2 per switch) - 4052031850
Arc Shield (2 per switch) - 4052085601
Load Base Assembly (2 per switch, incl. lugs, does not incl. class T fuse adapter) - 4052112050
Load Base class T fuse adapter (1 per load base assembly) - 4052038150
Load Base Mounting Screw (3 required per load base) - 2142720241
Load Base Side Insulator (1 per load base) - 4052050850
Handle Knob Kit - 4028343550
Lug Assembly (per lug) - 4025128750
Lug Mounting Nut (per lug) - 2342702400



CTA-ID : 3229
Was this helpful?
What can we do to improve the information ?