Technical FAQs

Ask a Question

What are the repair parts for a QMB323HW, Series E1 (E01)?

Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4051239950
Load Base Assembly (1 required, includes lugs) - 4052068050
Load Base Mounting Screw (2 required per load base) - 2142717161
Handle Knob Kit - 4028343750

CTA-ID : 2861
Was this helpful?
What can we do to improve the information ?