Technical FAQs

Ask a Question

What are the repair parts for a QMB262T, Series D2 (D02)?

The QMB device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4051239950
Load Base Assembly (1 required, includes lugs) - 4056014050
Load Base Mounting Screw (1 required per load base) - 2142717161
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101652
Lug Mounting Nut - 2342501701

CTA-ID : 2836
Was this helpful?
What can we do to improve the information ?