Technical FAQs

Ask a Question

What are the repair parts for a QMB222HD, Series D2 (D02)?

Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4056669451
Load Base Assembly (1 required, includes lugs) - 4056002550K
Load Base Mounting Screw (1 required per load base) - 2142717161
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101652
Lug Mounting Nut - 2342501701



CTA-ID : 2834
Was this helpful?
What can we do to improve the information ?