Technical FAQs

Ask a Question

Are compression lugs available for LC LI, LE, LX, LXI I-Line breakers?

Issue:
Are compression lugs available for LC LI, LE, LX, LXI I-Line breakers?

Product Line:
Circuit breakers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
NO. They are available for the unit mount versions of these breakers only.
Note:  LE, LX, LXI are obsolete circuit breakers.


CTA-ID : 2280

Was this helpful?
What can we do to improve the information ?