Technical FAQs

Ask a Question

What are the repair parts for an EZM1400CB, Series M01 main circuit breaker unit?

Issue:
Previous design repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:

Cover (full length) - EZM1400CBC
Circuit Breaker Cover (plastic) - BCM
Cover Screws - 4020513002K
Main Circuit Breaker - LHP26400
Standard Lugs for Circuit Breaker (kit includes 1-lug) - AL400LA
Alternate Lugs for Circuit Breaker (kit includes 1-lug) - AL400LH7
Additional Lugs available for Circuit Breaker, refer to Digest
Neutral Lug (kit includes 3-lugs) - MMLK250
Alternate Neutral Lug (kit includes 3-lugs) - MMLK500
Bonding Strap - 7329696750
Mounting Channel - 7329654301
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP


CTA-ID : 3207
Was this helpful?
What can we do to improve the information ?