Technical FAQs

Ask a Question

Does a KA225F or KA225S circuit breaker enclosure provide the capability to padlock the circuit breaker in either the ON or the OFF position?

KA225F and KA225S enclosures provide an integral lock plate on the cover that allows the circuit breaker to be padlocked in the ON or OFF position. A Handle Padlock Attachment, HPAFK, could be purchased separately and field installed on the breaker to provide padlock capability in the ON or OFF positions.

CTA-ID : 2200
Was this helpful?
What can we do to improve the information ?