Technical FAQs

Ask a Question

Where do the AC Power Outlet Accessories, catalog numbers SDM4AC or SDM8AC, mount?

The SDM4AC or SDM8AC mount inside of the Structured Wiring enclosures, catalog numbers SDM18BW or SDM36BW. The AC Power Outlet Accessory can be mounted in any of the four corners of the enclosure. The SDM4AC will take up 5.5`` of grid mounting space. The SDM8AC will take up 11`` of grid mounting space (5.5`` on each side of the enclosure).

CTA-ID : 2187
Was this helpful?
What can we do to improve the information ?