Technical FAQs

Ask a Question

Can we spring return 2 positions on a cam switch?

Issue:
Can we spring return 2 positions on a cam switch?

Product Line: 
9003 Cam switches

Environment:
North American Products

Cause:
Would like multiple spring return positions 

Resolution:

No. With our cam switches we can only spring return from 1 position, and it can only be the outside position and switching angle can only be 30 degrees.
 
Was this helpful?
What can we do to improve the information ?