Technical FAQs

Ask a Question

What are the repair parts for a QMB265WT6, Series E1 (E01)?

Only the parts listed below are considered field replaceable:
Complete Arc Suppression Assembly - 2 part numbers required:
Arc Suppressor Assembly (2 per switch) - 4052028950
Load Base Assembly (2 per switch, includes lugs) - 4052054750
Load Base Mounting Screw (3 required per load base) - 2142720241
Load Base Side Insulator (1 per load base) - 4052083501
Handle Knob Kit - 4028343550
Lug Assembly - order Load Base Assembly



CTA-ID : 3195
Was this helpful?
What can we do to improve the information ?