Technical FAQs

Ask a Question

What are the repair parts for a PAK31C, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161 (2 Req`d)
Interior Trim - 4054028301
Interior Trim Mounting Screw - 4020513001K (2 Req`d)
Interior Assembly - 4054017851 (Includes the Base Assy, Circuit Breaker(s) and Receptacle(s) listed below. Also includes neutral assembly, not listed separately)
Interior Assembly Mounting Screw - 2142217101 (4 Req`d)
Base Assembly - 4054017750
Circuit Breakers - QO120GFI and QO230
Receptacle - 4054001450 (125 volt/20 amp) and 4054004250 (125/250 volt/30 amp)
Receptacle Mounting Screw - 2190312160 (1 req`d for the 125 volt/20 amp receptacle)
Receptacle Mounting Screw - 2159412120 (2 req`d for the 125/250 volt/30 amp receptacle)
Ground Bar - 4023089990
Ground Bar Mounting Screw - 2159414200 (1 req`d)
Neutral Bonding Screw - 4028318554
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241 (2 Req`d)
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 3183
Was this helpful?
What can we do to improve the information ?