Technical FAQs

Ask a Question

What are the repair parts for a SU3040D300K Series M01?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
meter cover - 40561-706-50
load center cover - 40561-361-52
Deadfront (interior Trim) - 40561-310-03
load center interior - 40558-425-50
meter base assembly - 58763-4 and 58764-4
mounting channel - 40561-420-03
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2752
Was this helpful?
What can we do to improve the information ?