Technical FAQs

Ask a Question

What is the lug wire range for a 30a safety switch, catalog number H221NRB ?

The lugs actual wire range is one #12-2 AWG (American Wire Gauge) Aluminum, or #14-2 AWG Copper. However, wire bending space limitations restricts the use to a maximum of #6 AWG. Refer to the latest Square D Digest, or to the Enclosed Safety Switches Catalog, document # 3100CT9801.

CTA-ID : 2144
Was this helpful?
What can we do to improve the information ?