Technical FAQs

Ask a Question

Can the GA-375T sensor be used with the GC200E relay?

No. This sensor is only compatible with the GA Ground Censor system. GC100 and GP sensors are compatible with the GC200 system.


CTA-ID : 2139
Was this helpful?
What can we do to improve the information ?