Technical FAQs

Ask a Question

Wants MTBF (Mean Time Between Failure) data for circuit breakers.

These measures are not designed for electro-mechanical devices and do not provide meaningful data. Circuit breaker life is more a function of number of operations, overloads, short-circuits, operating environment, etc. We have no MTBF numbers to offer.

CTA-ID : 2718
Was this helpful?
What can we do to improve the information ?