Technical FAQs

Ask a Question

What is the 380 volt replacement coil for a Type SA NEMA Size 00 contactor or starter?

The 380 vac replacement coil for all Size 00 (i.e., SA) contactors depends on the device`s series or revision. The following outlines the part by Series number: Series A 60 hz- 31041-400-56, 50-hz 31041-400-57 Series B - 60 hz- 9998SAC59. For enclosed devices, the series information is based on device and not enclosure nameplate.


CTA-ID : 4810
Was this helpful?
What can we do to improve the information ?