Technical FAQs

Ask a Question

What are the repair parts for a HOM816U200FTRB, Series S01 load center?

Issue:
Repair parts request

Product Line:
Homeline Load Centers

Environment:

Repair parts

Cause:
Maintenance on the device

Resolution:

Only the parts listed below are considered field replaceable:
Cover - 4054802204 (OBSOLETE AND NO LONGER AVAILABLE)
Cover Mounting Screw - 2142717161 (2 required)
Interior Trim - 4056544001 (OBSOLETE AND NO LONGER AVAILABLE)
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - HOM816U200FTRBI
Neutral Bonding Screw - 4028345850K
Main Lugs Kit/Main Breaker - This load center is a Universal Main device which has no Main Lug or Breaker installed. Field install QOL225 for main lug. Field install QOM2100VH (100 amp), QOM2125VH (125 amp), QOM2150VH (150 amp), QOM2175VH (175 amp) or QOM2200VH (200 amp) for main breaker.
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 3156
Was this helpful?
What can we do to improve the information ?