Technical FAQs

Ask a Question

Are accessories on LA or LH bottom-feed I-LINE circuit breakers field installable?<br />Suffix MT, LH36400MT, LA36400MT

No. Factory installed only. When the shroud is on the OFF end it covers up the normal port for the leads.


CTA-ID : 2694
Was this helpful?
What can we do to improve the information ?