Technical FAQs

Ask a Question

What are the repair parts for the QMB221TW, Series E1 (E01)?

The QMB device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield (1 required) - 4051254201
Load Base Assembly (1 required, includes lugs) - 4056002650
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101652




CTA-ID : 2692
Was this helpful?
What can we do to improve the information ?