Technical FAQs

Ask a Question

What is the replacement 277 volt coil for a Type SE NEMA Size 3 contactor or starter?

Use part number 31074-400-49 for 2 & 3 pole devices rated for 60 hertz. For 4 & 5 pole devices rated for 60 hertz, use part number 31091-400-49.



CTA-ID : 4783
Was this helpful?
What can we do to improve the information ?