Technical FAQs

Ask a Question

Will a LA11021 work an older LA36300?

This shunt trip will work on Series 4 or higher LA breakers. If the series number is not visible on the breaker, this shunt trip will work if the breaker has the accessory ports on the front of the breaker.

CTA-ID : 3143
Was this helpful?
What can we do to improve the information ?