Technical FAQs

Ask a Question

What is the red LED located in the black area near the long-time dials on a micrologic trip unit? It blinks and is on intermittently.

The LED is a fiberoptic port that is used for internal testing at the factory. It only indicates that enough current is going through the breaker to power the trip unit.


CTA-ID : 3113
Was this helpful?
What can we do to improve the information ?