Technical FAQs

Ask a Question

What are the repair parts for a RC12L200CH Series M01?

Issue:
Repair parts

Product Line:
CSED

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 4056167850 (Includes latch)
Load Center Cover - 4056157550 (Includes hinges and latch)
Load Center Cover Mounting Screws - (4) 2159417121
Dead Front Interior Trim - 4056173801
Dead Front Interior Trim Mounting Screws - 4020513001K (This kit contains 10 screws. Only 2 screws are required to mount the interior trim)
Load Center Interior - 40561-621-50
Load Center Interior Mounting Screws - (4) 2153217160
Meter Base Assembly - 4056190050 (Includes meter base, line side lugs, meter jaws, meter jaw blade guides and horn bypasses)
Meter Jaw - (4) 4052706950 (OBSOLETE - REPLACED BY 7329794850) (Line side meter jaws included in Meter Base Assembly)
Meter Jaw Mounting Keps Nuts - (4) 2342702001 (Line side meter jaw mounting keps nuts included in Meter Base Assembly)
Meter Jaw Blade Guide - (4) 4052761901 (Line side meter jaw blade guides included in Meter Base Assembly)
Line Side Horn Bypasses - (2) 4056150901 (Included in Meter Base Assembly)
Load Side Horn Bypass (Left) - 4052783101
Load Side Horn Bypass (Right) - 4052783102
Fifth Jaw Assembly - 4052797750
Fifth Jaw Assembly Mounting Screw - 2153217160
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2604
Was this helpful?
What can we do to improve the information ?