Technical FAQs

Ask a Question

What are the repair parts for an EZM11200FS, Series M01 main fusible switch unit?

Only the parts listed below are considered field replaceable:

Cover (full length) - EZM11200FSC
Cover Screws - 4020513002K
Molded Case Switch - PHF260000M
Fuses Required (order separately) Class T (300 Vac) 1200A max.
Alternate Lugs for Molded Case Switch (kit includes 1-lug) - AL2500PA
Additional Lugs available for Molded Case Switch, refer to Digest
Neutral Lug (kit includes 3-lugs) - AL2500PA
Bonding Strap - 7329696751
Mounting Channel - 7329654302
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP


CTA-ID : 5774
Was this helpful?
What can we do to improve the information ?