Technical FAQs

Ask a Question

What is the accuracy of the ALAM and ALAMP Local Current Meter trip indicator Kit?

The meter accuracy is + or - 2% of full-load current. The meter is less accurate at lower amperages and more accurate at higher amperages. However, total system accuracy is within +/- 7.5% when the current sensors are factored in. The current sensors measure the current on each phase of the breaker.


CTA-ID : 1698
Was this helpful?
What can we do to improve the information ?