Technical FAQs

Ask a Question

Will an 80% rated circuit breaker trip if 80% of its rating is exceeded?

No. The 80% rating is an NEC restriction designed to prevent over-heating and nuisance tripping of enclosed breakers and breakers in panelboards and switchboards which may experience a heat build-up due to air-flow restrictions and the thermal contributions of other breakers.


CTA-ID : 451
Was this helpful?
What can we do to improve the information ?