Technical FAQs

Ask a Question

How long will the current D-Line product be offered? When will the current line become obsolete?

Our obsolescence plan is as follows:

January 1, 2002 announce obsolescence and reduced availability of the current line. At that time we may increase the pricing of the current line to encourage conversion to TeSys.

January 1, 2003 announce that the current line is obsolete. We project that stock of current devices will be depleted.


CTA-ID : 1649
Was this helpful?
What can we do to improve the information ?