Technical FAQs

Ask a Question

What is the AIC rating of Class 8910 Type DPA contactors?

Issue:
What is the AIC rating of Class 8910 Type DPA contactors?

Product Line:
Definite purpose contactors

Environment:
Products sold and used in the United States

Cause:
Identifying AIC rating

Resolution:
AIC or Short Circuit rating is a function of the upstream protective device. The DPA device conforms to the UL Standard for withstandability which is as follows; devices with maximum horsepower rating of 1/2 to 50 horsepower 5,000 amps, devices with maximum horsepower rating of 51 to 75 horsepower 10,000 amps.


CTA-ID : 1641
Was this helpful?
What can we do to improve the information ?