Technical FAQs

Ask a Question

How is a DRK600 Class R Fuse Kit assembled to the General Duty switch fuse clips?

Product design features

Product Line:
General Duty Safety Switches

Class R fuse kit installation



The DRK600 consists of a three rejection pins and collars. The rejection pin is inserted into a hole in the LINE SIDE fuse clips, adjacent to the switch blade hinge. Once the rejection pin is inserted into the fuse clip, the collar is then pushed onto the rejection pin. A pair of pliers may be required to push the collar onto the rejection pin. The rejection pin should not be able to be removed once properly installed.

CTA-ID : 1594
Was this helpful?
What can we do to improve the information ?