Technical FAQs

Ask a Question

How is a DRK40 Class R Fuse Kit installed into the correct General Duty switch fuse clips?

Issue:
Product design features

Product Line:
General Duty Safety Switches

Environment
Class R fuse kit installation

Cause:
application

Resolution:

The DRK40 is a rejection pin inserted through a hole in the switch LINE SIDE fuse clips and pushed into a collar located on the switch blade hinge pin. The rejection pin should not be able to be removed once properly installed. Three rejection pins are included in each kit.


CTA-ID : 1590
Was this helpful?
What can we do to improve the information ?