Technical FAQs

Ask a Question

What is the part number for an auxiliary contact for NEMA contactors & starters?

Class 9999Type SX6 (N.O.) or Class 9999 Type SX7 (N.C.) or Class 9999 Type SX8 (N.O. & N.C.). These contact units are external mounted and are field convertible. For additional auxiliary contact options see Auxiliary contacts in the Class 9999 Accessories section of current Digest.


CTA-ID : 1532
Was this helpful?
What can we do to improve the information ?