Technical FAQs

Ask a Question

What is the Solid Neutral Assembly for use in a LA400F, LA400S or LA400R enclosure when using a 250 ampere, KAL circuit breaker?

When using a 250 ampere KAL circuit breaker in the LA400F, S or R enclosure, you should use the 400SN Solid Neutral Assembly. If using a 225 ampere, or smaller, KAL circuit breaker in the LA400F, S or R enclosure, you should use the SN225KA Solid Neutral Assembly.


CTA-ID : 1491
Was this helpful?
What can we do to improve the information ?