Technical FAQs

Ask a Question

Are molded case circuit breakers repairable?

Product Line:
Molded Case Circuit Breakers

Environment:
Molded Case Circuit Breakers

Cause:
Need to know if breaker can be repaired.

Resolution:
Molded case circuit breakers are not repairable. Certain parts such as lugs, electrical accessories, handle extensions, and trip units might be replaceable depending on the breaker type. Please check based on breaker and accessory type to see if replacement of that part is possible.
Was this helpful?
What can we do to improve the information ?