Technical FAQs

Ask a Question

Are multiple equipment ground wires (bare or green insulated) allowed to be terminated in an Equipment Ground Bar of a QO or Homeline loadcenter?


Product Line:
LC Accessory

Wiring clarification

The terminals of an Equipment Ground Bar for use in QO or Homeline loadcenters are listed and labeled to accept one or two #14 - #12 AWG copper; or, one or two #12 - #10 AWG aluminum ground wires. Terminals may accept only one ground wire per terminal #10 - #4 AWG copper or one #8 - #4 aluminum ground wire.

CTA-ID : 176
Was this helpful?
What can we do to improve the information ?