Technical FAQs

Ask a Question

Where can I get a binded manual for an 8804 type 1CC04B SERIES A omegapak drive?

The service bulletin number for this manual is 8804-3.  This binded manual is stil available through the Literature fulfillment center at 1-800-888-2448 for Internal and 1-800-392-8781 for customers.

Also, the manual can be obtained by going to SquareD.com.  At the home page select country of ``United States`` then click Go!  At next page will go under Customers & Markets section and click on ``Industrial``.  At next page will go under resources and click on ``Product Technical Library``.  At next page will scroll down to Motor Control Section and click on ``AC Drives``.  At next page will scroll down to bottom of Subcategories and click on ``Obsolete Products``.  Then you will select the appropriate product under the subcategory and click on that product.  At the next you will go under the Publications tab and select the desired bulletin.


CTA-ID : 1350
Was this helpful?
What can we do to improve the information ?