Technical FAQs

Ask a Question

Why won`t the ALAM ammeter display read current on each phase. Pressing the reset button causes the battery-good symbol to come up.

The circuit breaker may not be carrying enough current to power the trip unit. It may need as much as 10--20% of rating before it will read.


CTA-ID : 7757
Was this helpful?
What can we do to improve the information ?