Technical FAQs

Ask a Question

What wire sizes can be used with the M9 IEC 947-2 Rated NC100LS Circuit Breaker?<br />

Cable range : pressure terminals are suitable for solid copper cables:
10 to 63A : 25mm^2 stranded or 35mm^2 solid


CTA-ID : 6258
Was this helpful?
What can we do to improve the information ?