Technical FAQs

Ask a Question

Is an early-break contact available for the NSJ rotary handle?

Yes, both an early-break contact 32605 and early-make contact 29346 is available for the NSJ rotary handle. This is also good for the NSJ400, NSJ600, and the NS400 and NS630 IEC frames.


CTA-ID : 5851
Was this helpful?
What can we do to improve the information ?