Technical FAQs

Ask a Question

What is the lug temperature rating on a LIL circuit breaker?<br />

The LIL termination is rated at 75 deg. C.


CTA-ID : 5575
Was this helpful?
What can we do to improve the information ?