Technical FAQs

Ask a Question

What is the part# for a key for a XCKP591 application? Specifically, the key housing mounts to the vertical face of a hinged door so that the key enters the keyway as the door swings to its closed position.

Suggested XCKY03. This key pivots in its housing as the key moves through its arc, so that side loads on the keyway are minimal. Fixed, non-pivoting keys, will cause the head of the switch to break due to side loading.

CTA-ID : 1081
Was this helpful?
What can we do to improve the information ?