Technical FAQs

Ask a Question

Is there a concern with the LH4N if the power is switched to emergency power after 2 seconds and the motor is still spinning?

Told him the LH4 will trip in such a situation.

CTA-ID : 7537
Was this helpful?
What can we do to improve the information ?