Technical FAQs

Ask a Question

Why does the LH4N not seam to ramp the motor up no mater how long the ramp?

Discussed with him the fact that with a starter, as the voltage ramps up, depending on load on the motor it can get to full speed long before the starter has finished the voltage ramp.

CTA-ID : 7532
Was this helpful?
What can we do to improve the information ?