Technical FAQs

Ask a Question

How does the end of start up relay work on the LH4N2?

The end-of-start up relay is installed on the side of LH4N2. When the unit comes up to speed, the shorting contactor pulls in and activates the end-of-startup relay.

CTA-ID : 7527
Was this helpful?
What can we do to improve the information ?