Technical FAQs

Ask a Question

Can you run 4 motors on one LH4N1 unit?

Need to add the FLA of the motors and make sure the softstarts` current rating can handle it. You would need separate overloads. Make sure all will be started at rthe same time.

CTA-ID : 7518
Was this helpful?
What can we do to improve the information ?