Technical FAQs

Ask a Question

LA36200, will this breaker mount into the same space as a LA36400?

Yes, 125 amp through 400 amp LA breakers have the same dimensions.


CTA-ID : 2089
Was this helpful?
What can we do to improve the information ?