Technical FAQs

Ask a Question

What are the Electrical Interlock Kits for the HU361, Series E2 and HU361EI Series E2 safety switches?

Issue:
Product Design features

Product Line:
Heavy Duty Safety Switches

Environment:
Electrical interlock accessories

Cause:
Application

Resolution:
Use the EK3001 for 1NO/1NC contacts and use the EK3002 for 2NO/2NC contacts. 

NOTE: the HU361EI comes with the EK3001 Factory installed and the above would be the replacements.

 
Was this helpful?
What can we do to improve the information ?